Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the power connector of the XBTGT7340?
Issue:
Need a replacement power connector for Magelis XBTGT

Product Line:
XBTGT5330, XBTGT5340, XBTGK5330, XBTGT6330, XBTGT6340, XBTGT7340

Resolution:
The replacement part number for the power connector of the XBTGT5/6/7 range is XBTZGPWS2. The product is a pack of 5 connectors.

The Phoenix Contact part number for the Schneider Electric part is: 1848009 (GMVSTBW 2.5-7.62)