How can we help you today?

Control Expert 14 returns 'Unknown fatal exception' error when creating a new application after closing an existing one.

Issue
Control Expert 14 returns 'Unknown fatal exception' error when creating a new application after closing an existing one.

Product Line
Control Expert 14

Environment
Windows 7, windows 8, Windows 10

Resolution
The issue is due to a bad installation of Control Expert.  The following steps can be used to resolve the issue:
  • Backup the saved applications.
  • Uninstall ‘Control Expert 14’
  • Uninstall the ‘EcoStruxture Control Expert PSx DTM Library’
  • Delete the folders that were left behind (C:\Users\Public\Documents\Schneider Electric\Control Expert 14.0)
  • Reboot the PC.
  • Clean out the 'C:\Users\SESA40~1\AppData\Local\Temp' folder.
  • Run a registry cleaner.
  • Reboot he PC
  • Reinstall Control Expert.
  • Retest.
  • Install the hotfixes in order (Run Control Expert after each install of the hotfix.)
  • Retest.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center