Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to set PID feedback assignment to Analog terminal in ATV310?

Parameter Reference channel 1 (401) must not set to 01, only to (163,164 or 183) so that parameter PID feedback assignment (59.00) can be changed from 00 to 01.
This is because you cannot use analog terminal for both reference and feedback at the same time.

1

2