Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the function of Cardew C Surge limiter?
Surge limiters are used on IT networks and installed at the output of the MV/LV transformer.
They protect ungrounded networks from overvoltages, that can be due to:
• internal breakdown of the MV/LV transformer
• lightning strikes on the upstream MV network
These overvoltages could have serious consequences and damage devices connected to the grid. The cardew will allow high energy overvoltages to flow to the earth, hence protecting the downstream
ungrounded network.