Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an INFG or internal error 16 on the ATV630 and ATV930 drives?
Issue:
What is the internal error 16 or INFG on the ATV630 and ATV930 drives?

Product Line:
Altivar Machines, Altivar Process Drives

Environment:
All model numbers, all serial numbers

Cause:
It can be caused by internal CPU error.

Resolution:
  • Verify that the option module is correctly connected to the slot.
  • Replace the option module.

Schneider Electric Egypt and North East Africa