Issue
Logging into FlexNet Publisher
Product Line
Power Monitoring Expert 9.0
Environment
FlexNet Publisher Login
Cause
Login credentials for FlexNet used in previous versions of PME won’t work for PME 9.0.
Resolution
1) First open the FlexNet Publisher page by going to http://localhost:8090 on your desired web browser.
2) Click on the 'Administration' tab located on the top right corner of the screen.
3) In the Sign In window input username and password based on set up explained below:
- If Floating License Mangaer is installed with the login "Domain\username" use the same format for the User Name field with the user's password.
- If it is local username then log in with "computer name\username" and user's password.
Note: This is only true for PME 9.0
Released for: Schneider Electric Egypt and North East Africa