Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the replacement connector kit for ATV340 drive?
Issue :
Replacement connectors for ATV340 drive.

Product Line :
Altivar Drive

Environment :
ATV340, Altivar Machine, Altivar 340

Cause :
Lost connector kit

Resolution :
There are three different part numbers for the kit, depending on the drive frame size.  A single connector piece is not available, order the complete kit only.

connector part photo 1

Drive Frame Size 1
Part# VW3A34001
ATV340U07N4 ATV340U15N4 ATV340U22N4 ATV340U30N4 ATV340U40N4

Drive Frame Size 2
Part# VW3A34002
ATV340U55N4 ATV340U75N4

Drive Frame Size 3
Part# VW3A34003
ATV340D11N4 ATV340D15N4 ATV340D18N4 ATV340D22N4

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center