How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the difference between P/N CCT15482 and P/N 15482? And are they compatible with analogue light sensor P/N CCT15263?

P/N CCT15482 is the new Acti9 IC100 twilight switch while P/N 15482 is the old platform IC100 twilight switch.

Old Platform P/N 15284 was delivered with a wall-mounted cell P/N 15268. P/N 15268 was never sold separately but only in combination with old platform IC100. If this cell got damaged, customer can order the spare wall-mounted cell P/N CCT15268.

New Platform P/N CCT15482 is delivered with a wall-mounted cell P/N CCT15268. P/N CCT15268 can be sold separately as a spare part.

According to the instruction sheet for Acti9 IC100 twilight switch P/N CCT15482, it is compatible with P/N CCT15263
https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=CCT15482_HW_all.pdf

However, the old platform of IC100 twilight switch P/N 15482 is not compatible with the new analogue light sensor P/N CCT15263.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center