Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
To do what, is used the mechanical thermostat NSYCCOTHC with Red button?

To heat the inside of an enclosure when T° is to low by starting a heater inside the enclosure.
This mechanical thermostat has a closed contact.
When the T° inside the enclosure is below the set point T°, the contact is closed and a heater is supplied.
When the T° inside the enclosure goes over the set point T°, the contact opens and the heater is stopped.