Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can customer replace graphical display of Altivar 71 with the graphical display of Altivar 340?

Graphical display for ATV71 is not compatible with ATV340.

Graphic keypad (VW3A1101) is compatible with Altivar 312 ,Altivar 61, Altivar 71, Altivar 32, Altivar 212, Altivar Lift, Altivar 61Q, Altivar 71Q, Altivar 312 Solar and Altivar Machine ATV320.

Another type of graphic keypad (VW3A1111) is used with ATV340 which is compatible also to Altivar process drives (600 and 900).

ATV71 HMI ATV600 HMI