Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the XBTF024110 Magelis HMI?

Article available in these languages: Spanish

Issue:
Replacement model for the XBT-F024 series Magelis HMI (XBTF024110, XBTF024310, and XBTF024510)


Product Line:
Vijeo Designer, XBTF, XBTL1000, HMIGK


Resolution:
The replacement for the XBT-F024 model series HMI (including part numbers XBTF024110, XBTF024310 and XBTF024510) is the HMIGK5310. The HMIGK5310 is programmed using Vijeo Designer V6.2 development software. The XBTF project must be converted to Vijeo Designer either manually or via the Schneider Electric Industrial Automation Tech Support.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa