Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find documentation for transformer/line loss calculation theory and methods for ION meters?

Issue
Clarify which meters support Transformer/Line Loss Compensation and which support Instrumentation Transformer Correction (ITC).

Product Line
ION7550, ION7650, PM8000, ION8650, ION9000

Environment
User Guide

Cause
Different meter models provide different compensation features. Users need to know which documentation to refer to for configuration and theory.


Resolution
Meters including ION7550, ION7650, ION8650, and ION9000 provide Transformer/Line Loss Compensation, whereas PM8000 meter provides Instrumentation Transformer Correction (ITC).

You can download the documentation for the Transformer/Line Loss Calculation theory and methods by clicking the following link ION meters.

For PM8000 Instrumentation Transformer Correction (ITC), refer to ION Reference document for detailed module operation.