Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Altivar 630 variable speed drive and EMC Category C3 IEC/EN61800-3 compliance. Maximum Motor Cable Length and dU/dt Filter necessity.
Altivar ATV630...N4 drives with integrated EMC filter meet C3 category with certain cable lengths and it varies with the drive size. For example ATV630U07N5...D45N4 allows max 150m shielded cable to comply C3, page 2/38 in ATV600 catalog 2021
But using additional EMC filter, the C3 category with up to 300m of shielded motor cable can be achieved. Page 2/39 in the catalog.

To meet EMC category, only following factors play role:
- drive type and size
- voltage
- shielded motor cable length
- additional EMC filter, if used

Nevertheless, long motor cable brings another drawback. It is not related to EMC, but to reliable operation:
- Higher leakage current and consequently overloading Altivar output IGBTs
- Possible overvoltage peaks on the motor terminals and motor wearing
- Voltage drop and worsen torque-speed performance
To reduce all these effects, Altivar output filter is strongly recommended. Criteria of motor cable length when output filter is not /is needed varies across the Altivar size and voltage. In general, start thinking about using output filter when motor cable length exceeds 50m. For 300m shielded cable at least dv/dt filter has to be used. Catalog specifies that 300m is the limit for ATV630...N4 + dv/dt filer. Sinus filter would be even better solution, but bear in mind that some drives needs derating if they are combined with sinus filter.


We have a customer who has to comply with EMC category C3 according to IEC/EN61800-3 with up to 300m of shielded motor cable for the ATV630…N4 product range (power ratings from U07 up to C11).

Schneider Electric Egypt and North East Africa