Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do Vijeo Designer Events have an Active state?

Issue:
When setting the "Alarm & Event List" to Active for an Event Group, nothing is display during runtime when there are Events. The only settings that display Events are History and Log.

Product Line:
Vijeo Designer (all versions)

Resolution:
Events in Vijeo Designer have no concept of "state". In essence, an event is something that has occurred already in the past. Therefore is no such thing as an Active event in Vijeo Designer. When using the Alarm & Event summary, the setting "Alarm & Event List" can only be set to History or Log for Events. If monitoring states is required, it is recommended to use Alarms rather than Events.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)