Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the available Motor Control Types in ATV600?

ATV600 drive embeds 5 motor control types which cover all the use cases depending on the application.

The following table shows the Motor Control types selection depending on the application needs:

CTT