Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VJD 6.2 license error with code 0X0000001E
1. Issue
For one customer, an error occurred in the VJD 6.2 license subsystem. the customer installed VJD V6.2, registered it and after the SP8 installation, he gets this error: See attached picture.
2. Environment
Vijeo Designer V6.2 SP8
3. Resolution
The license subsystem means that the license is corrupted. The resolution is to properly uninstall VJD, clean registers and delete the LC9xxxxxx.ocx file. ( c: \ Windows \ LC9GCN9J.ocx ).Then install VJD with proper license.


Schneider Electric Egypt and North East Africa

Attachment(s)
error1.png [36.67 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center