Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Quantum Battery Duracell CR-V3 - DL2/3A
Question:
Please confirm that for the item 990XCP98000, the battery manufacturer is DURACELL and the MFR.PART NO: DL2-3A
we are confused because of you check the below link. It is mentioned that the battery is a Duracell CR-V3.
https://www.se.com/ww/en/faqs/FA190511/
The customer requirement is a DL2-3A battery.

Answer:
For Quantum - 140 CPU65150, The part number for the battery is 990XCP98000, Lithium 3V Duracell (manufacturer part number DL2/3A).

CR-V3 is just another designation name for the Duracell Battery DL2/3A