This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The SE8000 Series Room Controller acts as a Modbus slave by using its RS485 port. As BACnet and Modbus use the same RS485 port, a setup menu allows switching between the two protocols.
The full register list can be found at Modbus Integration guides that can be downloaded from Exchange for SE8300, SE8600, SER8300 and SEZ8250.
Released for: Schneider Electric Egypt and North East Africa