Issue:
Two wire type to level control on the ATV600 Process drives.
Product Line:
ATV630 and ATV930 Process drives
Environment:
All
Cause:
Set two wire type to level to start on power up with start command
Resolution:
Programming example to set up 2 wire for level control.
Main Menu
Complete Settings
Command and References menu
Set 2-Wire type setting to LEL or Level
Done
ATV600 programming manual
https://www.se.com/ww/en/download/document/EAV64318/
Two wire type to level control on the ATV600 Process drives.
Product Line:
ATV630 and ATV930 Process drives
Environment:
All
Cause:
Set two wire type to level to start on power up with start command
Resolution:
Programming example to set up 2 wire for level control.
Main Menu
Complete Settings
Command and References menu
Set 2-Wire type setting to LEL or Level
Done
ATV600 programming manual
https://www.se.com/ww/en/download/document/EAV64318/
Released for: Schneider Electric Egypt and North East Africa