Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does EOTE V3.1support communication with M241 PLC via Somachine Network IP address
1. Issue
One customer asks if EOTE V3.1 supports communication with M241 PLC via SoMachine Network IP address. He finds it works via SoMachine Network NodeName but it does not work via IP address.
2. Environment
EOTE V3.1
3. Resolution

The reply from EOTE R&D is this is not EOTE's issue. It is M241's limitation. For M251, the symptoms can be resolved by updating the firmware on the PLC side.
4. FAQ Applicable Conditions
It also applies to VXD and EOTE V3.1 SP1.