How can we help you today?

How to access command line diagnostics in SCADAPack x70 RTU?

There are two main ways to access command line diagnostics:
1. Using an ASCII terminal connected to a SCADAPack serial port configured for the Cmd Line function. This is the method used to display startup diagnostics.
The Serial 4 is default Port function is Command Line.
command line
2. Using Telnet over TCP/IP links. Multiple Telnet sessions may be established with the SCADAPack on the same TCP/IP interface, or multiple sessions may be simultaneously established on multiple TCP/IP interfaces.

Enable the Telnet server under the IP Communication>Ethernet Ports>Services. Then hit apply button.

Telnet server

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center