Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does HMISTO715 support Modbus Function Code 23 in slave mode?
1. Issue
When HMISTO715 is configured as a Modbus slave, is it compatible with Modbus Function Code 23?
2. Environment
HMIST0715
3. Resolution
HMISTO715 supports Modbus SIO Slave Driver and this driver supports Modbus Function Code 23- Read/Write Multiple Registers. So HMISTO715 is compatible with Modbus Function Code 23 in slave mode.
4. FAQ Applicable Conditions
It also applies to HMISTO705 and HMISTO735.