Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the fuse type used in the GS2 Disconnect Switches?
Issue:
Need to know the fuse type for the GS2 Disconnect.

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
GS2 Fusible Disconnect Switches

Resolution:
GS2 rated from 30-60A will use a Cartridge Type fuse.  Switches from 100-800A will use a Blade Type fuse.