Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Limitations when Engineering a Multi-version EcoStruxure Building Operation System
From version 3.1 of EcoStruxure BMS it is possible to use a multi-version system. This means that you can have an 3.1 Enterprise Server with an attached 3.0 SmartX server.

There are some limitations when you engineer a multi-version system:

Copy and paste
It is not possible to copy and paste objects between servers with different versions.

Custom types
Custom types created in a higher version cannot be checked out on a server with a lower version. If you try to do this, you get the error message “Error dialog Object has wrong type or version at retype. Invalid Operation”

Import
Import can only be done to a higher or the same version.

Schneider Electric Egypt and North East Africa