Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can AR8654 be installed on the NetShelter Networking roof?
Issue:
There are places on the Networking roof where the AR8654 will not install.

Product Line:
NetShelter Networking Cabinets

Environment:
AR3140, AR3340, AR3347 all serial ranges.

Cause:
The Networking roof is different than the standard NetShelter roof.

Resolution:
Please see the attached file for locations where the AR8654 can mount.

Schneider Electric Egypt and North East Africa

Attachment(s)
AR8654 Installed Onto NetWorking Cabinet.pdf [226.31 KB]