Issue:
Are the electronics in the VW3A3616 conformal coated?
Product Line:
Altivar Process / Machine communications modules.
Environment:
All
Cause:
Conformal coating of the communication modules
Resolution:
Are the electronics in the VW3A3616 conformal coated?
Product Line:
Altivar Process / Machine communications modules.
Environment:
All
Cause:
Conformal coating of the communication modules
Resolution:
The communication modules of ATV320 and Altivar process are coated the same way as the Drives PCB.
Standard is :
- Chemical class 3C3 conforming to IEC/EN 60721-3-3 (1),
- Mechanical class 3S3 conforming to IEC/EN 60721-3-3 (1),
This protects the components against harsh environments such as humidity, pollution, thermal variations and shocks, vibrations and mechanical shocks.
Released for: Schneider Electric Egypt and North East Africa