Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Does ATV630 support constant torque applications which require a significant overload (up to 150%)?

Altivar Process variable speed drives are designed for use in two operating modes that can optimize the drive nominal rating according to the system constraints.

These two modes are:

  • Normal duty (ND):
Dedicated mode for applications requiring a slight overload (up to 110%) with a motor power no higher than the drive nominal power.
The drive is designed to run up to 60 s at 110% of nominal current.
  • Heavy duty (HD):
Dedicated mode for applications requiring a significant overload (up to 150%) with a motor power no higher than the drive nominal power derated by one rating.
The drive is designed to run up to 60 s at 150% of nominal current.

HD vs ND

Refer to attached document for Drive Ratings in Normal and Heavy Duty

Schneider Electric Egypt and North East Africa

Attachment(s)
Drive Ratings In Normal and Heavy Duty.pdf [1 MB]