Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The selection for the PMEPXM0100 module is grayed out in the 'New Device' window for the ERIO rack..
Issue
Cannot add a PMEPXM0100 Profibus module to an Ethernet Remote IO (ERIO) rack.

Product Line
PMEPXM0100

Environment
Control Expert 14.1

Resolution
An attempt to add a PMEPXM0100 Profibus module to an ERIO rack will result in the selection for the module
being greyed out and unavailable in the 'New Device' window.
gh


The reason tht this occursis because the 'PMEPXM0100 Profibus Module' is only supported on an ERIO rack with 'BMECRA31210 exec firmware version > 2.1'.


To resolve the issue,
  • Right click on the 'BMECRA31210'.
  • Select 'BMECRA31210 >= 2.10'.
ujio

  • Double click on an empty slot.
  • Add the PMEPXM0100 to the rack.
tyuio


Note:  The PMEPXM0100 is currently not available or supported on the ERIO rack of an M580 Hot Standby PLC