How can we help you today?

Channel output limit for the Pulse Width Modulation mode in the BMXEHC0200

Issue
Channel output limit for the Pulse Width Modulation mode in the BMXEHC0200

Product Line
BMXEHC0200

Environment
Control Expert, Unity

Resolution

When you choose to use the Pulse Width Modulation mode in the BMXEHC0200 configuration, the user manual does not specify
if the feature is limited to 1 or 2 outputs per channel.

The Pulse Width Modulation Mode (PWM) is limited to 1 output per channel.  In this operating mode (PWM), the module uses
an internal clock generator to supply a periodic signal at the module’s Q0 output. This only applies to the Q0 output. The Q1 output is
independent of this mode.

Since each counting channel has 2 outputs Q0 and Q1. The user is only allowed to use Q0 on each channel and not Q1.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center