How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the password set condition/rules need to follow to set the Micom P40 password with CSL0?

Issue/description:

Password set condition/rules need to follow to set the Micom P40 password with CSL0

Product family:

Easergy MiCOM Px4x relay

Resolution:

For Easergy MiCOM Px4x relay with CSL0, SAT is not supported for the configuration, so only the alphanumeric password can be used.

• The alphanumeric password is settable via Easergy Studio and the Front panel
• Passwords may be any length between 1 and 16 characters long
• Passwords may contain any ASCII character in the range ASCII code 33 (21 Hex) to ASCII code 122 (7A Hex) inclusive
• No password compliance is required
• The alphanumeric password will used for Courier access and the front panel access Arrow key password is not available for relay with CLS0.

Important Note:
The Schneider Electric password policy is one of the key elements of the Cyber
Security Policy.
Good practice to improve the Password definition:
- Use common Cyber Security Good Practice for password complexity definition
by using strong passwords.
- Change All Passwords from their default value when taking the protection device
into use. (User must change password after first login).
- Change Passwords regularly. (User must update password after a certain period
of time).
- Use NERC Compliant password as much as possible.
- Enforce the use of strong and complexes Password as : Caps characters +
Lowercases characters + Numbers + Special characters in one password.
- Set the minimum password length to 10 characters.
- Switch off all Comm port not use on the device, if possible.
- Do not reuse old passwords.
- All P40 relays installed before January 2020 should be checked separately case by
case to confirm the Cyber Security conformity to Standard/country law.
All user must be aware of best practice concerning passwords, these include:
- Not Sharing personal passwords.
- Not displaying passwords during password entry.
- Not transmitting passwords in email or by other means.
- Not saving the passwords on PC’s or other devices.
- Not written password on any supports.
- Regularly reminding users about best practices concerning password.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center