Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
HVAC Heat and Flow Meter Selection

"Heat and Flow Meter Selection tool" is publicly available webtool that can be used desktop computers as well as mobile devices 10” or larger, with the latest browsers and their updates applied. The selection tool is a great resource to help choose the right heating/cooling meter for your application.
Selecting the right meter for your application is simple and straight forward. Within just 5 ‘clicks’ (tick boxes) the right product is displayed automatically. All that is required is:

  • Flow Meter Type - Heating or Cooling
  • Nominal Flow (m3/h)
  • Meter Size/Connection
  • Installation - in the Flow or Return
  • Communication Protocol/Type (optional)


The tool also provides a very useful compare facility to assist with further narrowing the correct part number selection.

Flow and heat meters selection tool


The full technical specifications, datasheets, CE certificates and environmental declarations will be available once the right meter has been selected. Whilst every effort has been made to provide useful and accurate information, it is strongly recommended that the detailed specification of the selected products be carefully and thoroughly reviewed before purchasing the items.

The tool can be accessed from the following link:
https://ecobuilding.schneider-electric.com/product-selection-tool/heatflowmeters