Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I have Advanced Display V3 connected to my EBO server, do I need a client license?
SmartX Advanced Display v3 (AD v3) is an industrial-grade Human Machine Interface (HMI) that can easily be locked to an application such as EcoStruxure Building Operation WebStation to create a dedicated tool for local operation and maintenance of an EcoStruxure BMS. When connected to EcoStruxure BMS server, AD v3 is counted as one WebStation client. Part of the new pricing model includes in client licensing the WebStation client. Starting from EBO v2, The WorkStation Standard and the WebStation will both be considered a client, and each will require a concurrent license to be able to log into the system. Three client licenses are included with each Enterprise Central and each Enterprise Server. When logging directly into a SmartX server, the number of WebStation connections is limited only by the Architectural Guidelines*. So, client license is only needed if AD v3 is connected to Enterprise Server or Enterprise Central directly.

*EBO 3.1 builds in the removal of any need to activate a Client feature license on SmartX servers to be able to connect WebStation to a SmartX server and log in. Where 3.0.4 and 3.0.3 with hotfix accomplished the same functionality, they did so by stating that 99 clients were available.

Schneider Electric Egypt and North East Africa