Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the chassis of the Easypact MVS and Masterpact NW ACB the same? If not, is there any retrofit kit to convert between NW Chassis into MVS Chassis?
The chassis of MVS is not the same as that of NW. Unfortunately, there is no retrofit kit to convert NW chassis into MVS chassis.