Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Current Limit range for ATS48 Softstarter?
Issue:
What is the minimum and maximum setting for Current Limit on ATS48 Softstarter?

Product Line:
ATS48, Altistart 48

Environment:
All

Cause:
NA

Resolution:
It is adjustable from 150 to 700% of In setting. However, maximum is limited to 500% of rated softstarter current.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center