Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the factors to consider in selecting the braking resistor for Altivar drives?
Issue:
What are the things to consider in selecting the braking resistors for Altivar drives?

Product Line:
All Altivar Drives

Environment:
All

Cause:
Needs to know if the factors to consider in selecting the braking resistor for Altivar drives

Resolution:
1.) Resistance - Choosing a too low resistance may damage the drive.  Too high and it's not as effective as a brake.  That's because higher resistance means we will get lower current from the drive.  Lower resistance means higher currents and too high current can damage the braking IGBT in the drive.

2.) Watts - Higher wattage means more durable braking resistor.

Schneider Electric Egypt and North East Africa

Attachment(s)
POWEROHM_SELECTION AND PRICE GUIDE_Y13M03D15.xlsx [1.38 MB]