How can we help you today?

Unable to save Realflo file and missing .TFV and .TFX files

The following error messages appear when saving the Realflo files.
PIC1
PIC2
Solutions:
Verify that the MSXML files are present in Programs and Features under the Control Panel.
PIC3
If these files do not appear under Programs and Features:
Download and install the msxml4.dll from the Microsoft website. Copy the file msxml.msi to the local PC and run it as administrator for the customer which have no MSXML 4.0 Parser shown in Control Panel. After that, check the Control Panel again to see if it shows up.

Alternatively, upgrade the Realflo to the latest version, https://www.se.com/us/en/download/document/Realflo_Flow_Computer/

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center