Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the meaning of the “Safety time before start” in SEPAM 80 relay when we work with SFT 2841 ,V15.0 ?
“ Safety time before start” it means time which inhibit closing output(o2) is set to 1.

After this time 49RMS unlatch the inhibit closing signal(Normally in SEPAM 80 is output O2).

O2 is used for inhibit closing signal. And it is set to Normally Close output  (inside the matrix_logics)