Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is it possible to simulate drive protection through SoMove software?
SoMove is the user-friendly setup software for PCs designed to configure Schneider Electric's motor control devices such as Altivar drives.

It incorporates various functions for the device setup phases such as:
• Prepare the device configuration offline, to optimize time spent on the field
• Simplify device start-up, commissioning and test
• Perform application tuning using scope meter
• Access device detailed maintenance data

While connecting the SoMove to the drive “Online Mode”, customer can monitor all required parameters and actual operating signals such as “motor current, speed, voltage, Input & Output IOs” simultaneously.

Also, supervising the drive actual status “OFF, Ready, Run or Fault”

If the drive tripped due to some protection activation like “Overvoltage, Overcurrent, Overload…. etc.”, the customer can notice this action through the SoMove platform beside the drive graphic keypad.

Indeed, it is not possible to make the drive trip in a virtual protection activation through SoMove software as these protections count on the drive hardware sensing thresholds and not be adjusted via software.

As clarified, customer can simulate drive voltage protection activation using a variable DC power supply, but it is rarely used for this purpose, it is used for drive capacitor reforming which has been stored for long period.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center