Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the drop-out voltage limits for TeSys D contactors?
For the AC control circuit characteristics for TeSys D drop out voltage ranges from 0.3 to 0.6 Uc at 60 °C  for D09 to D80A , 0.3 to 0.6 Uc at 55 °C for D80 to D95 and 0.3 to 0.5 Uc at 55 °C for D115 and D150.

While for DC controlled circuit, the drop out ranges from 0.1 to 0.25 Uc at 60 °C for LC1 D09…D38 and LC1 DT20…DT40, 0.1 to 0.3 Uc at 60 °C for LC1 D40A…D80A LC1 DT60A and DT80A,
0.1 to 0.3 Uc at 55 °C for LC1 or LP1 D80 and LC1 D95 and 0.15 to 0.4 Uc at 55 °C for LC1 D115 and LC1 D150.
refer to attachment

Schneider Electric Egypt and North East Africa

Attachment(s)
TeSys D contactors drop-out voltage limits.pdf [641.21 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center