Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
For Switch disconnector, can I use 3P+N instead of 4P since both doesn’t provide protection for neutral pole?
Issue: Can I install the neutral conductor on any pole?
Environment: iSW Switch disconnector.
Resolution: For switch-disconnector iSW-NA ref. A9S70xxx, products are 1P+N or 3P+N. According to IEC 60947-1 std §7.1.9, Neutral pole identified by letter N (left side pole of the product) closes before and open after the Phases poles. This is to guarantee preventing floating voltages in 3P+N network.