Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is EBO WebStation Kiosk mode and how to enable it?

Issue:
Want more information about WebStation Kiosk mode.

Product Line:
EcoStruxure Building Operation, WebStation

Resolution:
By enabling EcoStruxure Building operation WebStation Kiosk mode, toolbars will be removed. This mode is best used with SmartX HMI Kiosk, you can use SmartX HMI Kiosk to lock AD v3 in Kiosk mode to help prevent users from accessing an app other than the one you have selected.

WebStation without Kiosk mode:
Webstation without kiosk mode

WebStation with Kiosk mode:
Webstation with kiosk mode
To enable WebStation Kiosk mode, You can append the WebStation kiosk mode parameter to the IP address, ex. 192.168.42.116 /?kiosk# .