Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Treck TCP/IP Ripple 20 Vulnerabilities Affecting Schneider Devices
Issue
What Schneider devices were affected by the Treck Inc. Ripple 20 Cyber Vulnerabilities

Product:
Schneider Devices

Environment
Cyber Security

Cause
Treck has disclosed 19 different vulnerabilities existing in its TCP/IP stack. These vulnerabilities range in severity and at least two could lead to remote code execution. Other potential impacts of these vulnerabilities include privilege escalation, denial of service, and information leakage.

Resolution
A list of Schneider Devices that are affected can be found in the document below.







Schneider Electric Egypt and North East Africa

Attachment(s)
SEVD-2020-175-01_Treck_Vulnerabilities_Ripple20_Security_Notification_V1.1.pdf [219.24 KB]