Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
SoMachine Basic is reading Modbus devices registers in reverse order.
Issue:
SoMachine Basic is reading Modbus devices registers in reverse order.

Environment:
SoMachine basic

Resolution:
SoMachine READ_VAR function block reads register as Mid-Little Endian (CDAB). Many Modbus devices can send data in a Big Endian (ABCD) format.
This means the SoMachine Basic software will list the least significant word first (%MWi) followed up by the most significant word (%MWi+1).
This can be resolved through changing the Modbus device settings, the gateway settings or through additional functions in SoMachine Basic. (For example, you can use a concatenate function to list the most significant word before the least significant word)