Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the syslog messages on BMENOC03x1 module?
Issue
Customer wants to know what are the syslog message list generated by the BMENOC03x1 module.

Product Line
BMENOC0301, BMENOC0311

Environment
Firmware 2.17

Resolution
The "BMENOC03x1 syslog messages – V2.pdf" document contains the Syslog messages generated by the BMENOC03x1 and sent to a syslog server.

Here is below the legend to read the document (extract from the document: Modicon Controllers Platform - Cyber Security - Reference Manual: EIO0000001999.06)
Events Logged
Syslog message structure:
FieldDescription
PRIFacility and severity information (description provided in following tables).
VERSIONVersion of the syslog protocol specification (Version = 1 for RFC 5424.).
TIMESTAMPTime stamp format is issued from RFC 3339 that recommends the following ISO8601 Internet date and time format: YYY-MM-DDThh:mm:ss.nnnZ
NOTE: -, T, :, . , Z are mandatory characters and they are part or the time stamp field. T and Z need to be written in uppercase. Z specifies that the time is UTC.
Time field content description:
YYY Year MM Month DD Day hh Hour mm Month ss Second
nnn Fraction of second in millisecond (0 if not available)
HOSTNAMEIdentifies the machine that originally sent the syslog message: fully qualified domain name (FQDN) or source static IP address if FQDN is not supported.
APP-NAMEIdentifies the application that initiates the syslog message. It contains information that allows to identify the entity that sends the message (for example, subset of commercial reference).
PROCIDIdentifies the process, or entity, or component that sends the event. Receives NILVALUE if not used.
MSGIDIdentifies the type of message on which the event is related to, for example HTTP, FTP, Modbus.
Receives NILVALUE if not used.
MESSAGE TEXTThis field contains several information:
  1. Issuer address: IP address of the entity that generates the log.
  2. Peer ID: Peer ID if a peer is involved in the operation (for example, user name for a logging operation). Receives null if not used.
  3. Peer address: Peer IP address if a peer is involved in the operation. Receives null
if not used.
  1. Type: Unique number to identify a message (description provided in following tables).
  2. Comment: String that describes the message (description provided in following
tables).


Syslog message facility values as per RFC 5424 specification associated with events type:
Facility valueDescription
0Kernel messages.
1User-level messages.
2Mail system.
3System daemons.
4Security / authorization messages.
5Messages generated internally by syslog.
6Line printer subsystem.
7Network news subsystems.
8UUCP subsystem
9Clock daemon.
10Security / authorization messages.
11FTP daemon.
12NTP subsystem.
13Log audit.
14Log alert.
15Clock daemon.
16...23Local use 0...7.

Syslog message severity values as per RFC 5424 specification associated with events type:
Severity valueKeywordDescription
0EmergencySystem is unusable.
1AlertAction must be taken immediately.
2CriticalCritical conditions.
3ErrorError conditions.
4WarningWarning conditions.
5NoticeNormal but significant condition.
6InformationalInformal messages.
7DebugDebug-level messages.

Schneider Electric Egypt and North East Africa

Attachment(s)
BMENOC03x1 syslog messages - v2.pdf [509.13 KB]