Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is it possible to connect PT100 RTD to ATS48?

Unfortunately, the PT100 RTDs are not compatible with the Altistart 48.

Only the PTC thermistor could be connected to PTC1 and PTC2.