{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PSO2020 with CU1 Easergy P3 default driver No Alarm log.
Issue:
Use default P3 driver in Profile editor.

Simulate alarm for this tag which is in the default driver but no alarm show up in PSO2020.

Simulate alarm in Easergy P3 and related alarm can be read by 3td party modbus test tool.
Request:


Response:

01 03 0A 04 C1 XXXX  04C1 whichi is for (Protection 50/51 Alarm) 1217

Cause: The root cause of this issue is the onboard alarms are disabled by default.

Answer:
The driver supports the download of on-board event logs. The device driver polls the device and checks for new log entries at regular intervals. The default polling interval is 500 m seconds.
Event log feature is disabled by default. To enable, set the parameter in the citect.ini file.
[Easergy.(cluster name).(equipmentName)]
EventLogEnabled=1.

Schneider Electric Egypt and North East Africa