Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via NMC times out


Issue:

XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via Network Management Card times out and is unable to complete

Product Line:

Smart-UPS Industrial

Environment:

XU1K3LLXXRCC and XU2K0LLXXRCC, All Serial Numbers

Cause:

When upgrading the firmware via the Network Management Card, there is a delay in transferring the data to the UPS.
This causes the update to time out and fail.

  • The time-out error occurs while Receiving Firmware image is in progress.
  • The percentage at which the time out error occurs varies from unit to unit.



The LCD Display on the UPS will look like this:
img



The NMC Web interface will display this error:

img

Resolution:

If you experience this issue, you can upgrade the UPS using a USB Thumb Drive rather than via the Network Management Card.
Instructions and the latest firmware image can be found in APC FAQ ID FA402857

Note: Subsequent UPS firmware updates can be performed via the NMC; however, the time to perform the update may increase by 10 minutes.