Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Hybrid DCS [2019] - How to activate the alarm of AALARM block that after transferring the application or power cycle the CPU?
  1. Issue

There are many Analog input instance used in customer’s project. Customer finds that after transferring the application or power cycle the CPU, the evaluation of an alarm conditions will be disabled. Since that customer need to enable the alarm by clicking the alarm enable switch on the Analog Input faceplate every time.

Since that, how to enable the alarm automatically after transferring the application or power cycle the CPU

  1. Product Line
HDCS2019, Citect 2018
  1. Environment
HDCS2019, Citect 2018
  1. Resolution

Please refer to AALARM_CFGW as the below screenshot indicates. Bit0 to Bit4 of the configuration word are used to enable or disable the alarm switch on the AnalogInput faceplate.

A screenshot of a cell phone  Description automatically generated
A screenshot of a cell phone  Description automatically generated
Customer can set the value of the configuration word to “31”. And you will find the evaluation of an alarm conditions will always be enabled.
A screenshot of a video game  Description automatically generated