Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Do you have 27R function (Remanent voltage / Anti-Backspin) function in Micom motor protection relay P24x relay range ?

Description:
27R function (Remanent voltage / Anti-Backspin) protection function in Micom P24x relay

Product family:
Micom 24x relays

Resolution:
27R function (Remanent voltage / Anti-Backspin) need to have option for VT connection = 2VT + Remanent.Yes, this option is available in Micom P24x