Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - I have created two Logical Devices, both of which map the same register from the same physical meter, but the logged data is only available for one of the Logical Devices

Issue
It is possible to create a Logical Device and map a register from a meter that is the input to a Data Recorder on that meter, then create a second Logical Device that includes the same mapping, i.e. the same physical meter register is used in two different logical devices. If this is done, only one of the Logical Devices will include logged data from the mapped register.

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Management Console

Cause
When this is done, two different entries are made in the IAS_MeasurementAddress SQL database table, but both point to the same underlying physical register originating from the device. If this is done, the logged data is only assigned to one of the Logical Devices, and which one gets the data seems to be random.



Resolution

PME 2020 and older:

The user should delete the Logical Device for which the logged data is not required.

PME 2021 and newer:


The system guide states the following:

When a logical device is configured, historical data for an output register (that is, an output measurement) on the physical device is automatically routed to the corresponding output measurement on the logical device.

When a logical device is configured, historical data is logged to the logical device and not the related physical device.

If multiple logical devices include the same input measurement from the same physical device, historical data from that input measurement is routed to the logical device that was configured last.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: